AXIS#.MOTOR.TBRAKEAPP
Description
This parameter is the mechanical delay required for the motor brake to close. When disabling an axis, the drive will servo to hold position for this time delay, allowing the brake to apply.
-
-
If AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter will be automatically configured for Kollmorgen motors.
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
ms |
|
Range |
0 to 1,000 ms |
|
Default Value |
75 ms |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.TBRAKEAPP | 0x500B | 0x1A | UINT | - | - | RW | False |
| AXIS2.MOTOR.TBRAKEAPP | 0x510B | 0x1A | UINT | - | - | RW | False |